This is release 1.10 of the MPC5553, MPC5554, MPC5533, MPC5534, MPC5561, MPC5565, 
MPC5566 and MPC5567 header files.
==============================================================================

This package is intended to assist in writing programs for the mpc5553/4 
mpc5533/4 and mpc5561/5/6/7  It consists of 8 header files: mpc5553.h, mpc5554.h, 
mpc5533.h, mpc5534.h, mpc5561.h, mpc5565.h, mpc5566.h, mpc5567.h plus a file that
defines standard types typedefs.h and a file which defines the CPU SPR registers.

Also included are integration specific vars files. These define variables used
by the eTPU APIs

The mpc5554.h defines all of the registers and bit fields in the mpc5554 device.
The mpc5553.h defines all of the registers and bit fields in the mpc5553 device.
The mpc5533.h defines all of the registers and bit fields in the mpc5533 device.
The mpc5534.h defines all of the registers and bit fields in the mpc5534 device.
The mpc5561.h defines all of the registers and bit fields in the mpc5561 device.
The mpc5565.h defines all of the registers and bit fields in the mpc5565 device.
The mpc5566.h defines all of the registers and bit fields in the mpc5566 device.
The mpc5567.h defines all of the registers and bit fields in the mpc5567 device.

The bit fields should be used carefully. Generally bit fields should only be used
when you want to read or write to a single bit field in a register. If you want
to access multiple bit fields in a register then an access to the complete
register should be used.

If you use the bit field to write to multiple bit field in a register then each
access with be done as a separate operation because generally the registers are
declared as violate. This could cause the code generate to be larger than if the
complete register was accessed.

This release contains:
mpc5533.h       version 1.6
mpc5534.h       version 1.5
mpc5553.h       version 1.7
mpc5554.h       version 1.6
mpc5561.h       version 1.1
mpc5565.h       version 1.3
mpc5566.h       version 1.3
mpc5567.h       version 1.4
mpc5533_vars.h  version 1.1
mpc5534_vars.h  version 1.1
mpc5553_vars.h  version 1.1
mpc5554_vars.h  version 1.1
mpc5561_vars.h  version 1.1
mpc5565_vars.h  version 1.1
mpc5566_vars.h  version 1.1
mpc5567_vars.h  version 1.1
mpc5500_spr.h   version 1.5
typedefs.h      version 1.4
readme.txt      this file.


History
------- 
Changes in 1.10
----------------
Added support for mpc5561.
PDI - Created module.h file for PDI module
FLEXRAY - MBSSUTR, MBIVEC & RSBIR bit field sizes updated. RSBIR, SELEC changed 
to SEL & RFRFCFR, FNUM changed to SEL to align with documentation.
eDMA - Updates to TCD's and the following registers: CR, ESR, SERQR, CERQR, 
SEEIR, CEEIR, CIRQR, CER, SSBR, CDSBR. HRSH/L Registers added.
XBAR - MPR5 & SGCPR5 added for PDI.
SIU -  ENGDIV bit field size modified.

Changes in 1.9
----------------
Added support for mpc5566.
FlexCAN - Changed bit name from BCC to MBFEN to reflect manual.
FlexCAN: Added the following bits :
MCR bits WRNEN & SRXDIS, CR Bits TWRNMSK & RWRNMSK and ESR Bits 
TWRNINT & RWRNINT added for MPC5533/34 and MPC556x (These bits are not 
present on Pre Rev A MPC5533/34).
FlexCAN: Removed CAN_E for MPC5566.
SPR: Added L1CSR0[WAM] & L1CSR0[CORG], L1SCR0[DPP] changed to DPB to 
align with documentation.  
mpc5533/4.
FLASH: MCR[PRD] bit added, BIUCR2 Register added, BIUCR_DPFEN & IPFEN updated.  

Changes in 1.8
----------------
Fix error in Flexcan BCC field for mpc5565/7.
Change __GHS__ to __ghs__ in typedefs.h

Changes in 1.7
----------------
Added support for mpc5565 and mpc5567.
For mpc5533/4 and mpc5553 header files:
	Fix typo in BIUPAR field width.  
Various changes to support new build methodology. This means that
many of the reserved field widths are declared differently. Register 
postions did not change.
 
Changes in 1.6
----------------
Corrections to PBRIDGE MPCR/OPCAR/PACR registers.
Affects mpc5554/53/33/34.h

Changes in 1.5
----------------
Added support for mpc5533 and mpc5534.
Fixed issues with FEC offsets in mpc5553.h. Also added RMON_R_DROP register 
which was missing.
Extended the PCR/GPDI/GPDO arrays to be as big as they can be (512/256/256)
     (MPC5533/4 uses PCRs 336,338,339,340/1/2 for CAL).
Added M4PFE to BIUCR and M4AP to BIUAPR for MPC5553. Also included in MPC5533/4

Changes in 1.4
----------------
Added EBI CAL support for MPC5553. 
Fixed address of FSBMCR.
No changes for MPC5554.
 
Changes in 1.3
----------------
1. Reverted to having seperate var files for mp5553/4. i.e mpc5553_vars.h and mpc5554_vars.h. 
   Due to different amount of Dtaa RAM.
2. Removed mpc5500_vars.h from the release.
3. Fixed mpc5553.h so that it has FLEXCANB removed and FLEXCANC included.

Changes in 1.2
----------------
1. Made mpc5500_spr.h the same as the version published in the config project on 
   the extranet.

Changes in 1.1
----------------
1. Prepended SPRs with "SPR_" in mpc5500_spr.h
2. Fixed copyright date in mpc5500_spr.h and mpc5500_vars.h 

Changes in 1.0
----------------
1. Added mpc5553.h
2. Renamed mpc5554_spr.h to mpc5500_spr.h
3. Renamed mpc5554_vars.h to mpc5500_vars.h

Changes in 0.17
---------------
1. Moved eTPU variable definitions to a seperate new file.
2. Removed SIU variable the GPIO routines do not need it.

Changes in 0.16
---------------
1. Fixed comments.

Changes in 0.15
---------------
1. Added support for new eTPU utilites routines. This required adding some
    variables to help define the eTPU module.
2. Updated the FlexCAN buffer ID field. The bit fields were defined. This may
    cause some compatibility problems because the ID field is now ID.R.

Changes in 0.14
---------------
1. All files updated for CVS version control and checked into repository.
2. Added ETPU_CODE_RAM definition.
3. Updated copyright from Motorola to Freescale.
4. Added new SCMOFFDATAR register to eTPU.
5. Fixed REDCR_A&B bit fields in eTPU.
6. Added new DBR bit in CTAR register for DSPI modules.
7. Included new mpc5554_spr.h file.
8. typedefs.h updated only for CVS no code changes.

Changes in 0.13
---------------
1. Fixed size of TIMER register in FlexCAN (was 16 now 32 bit).
2. Changed names of eTPU memory defines to start with ETPU so they
    do not get confused with the main cores memory

Changes in 0.12
---------------
1. Changed SERQR CERQR SEEIR CEEIR CIRQR CER SSBR CDSBR registers back to 8bit.
2. Changed DTRER to CDTRER and STACR to REDCR to match User manaul 1.1
3. Added mpc5554_spr.h file with support for CPU core SPR registers.
4. Some formal testing has been done on the mpc5554.h file (edma and etpu modules).
5. Bug tracking is now controlled by Bugzilla on a Motorola internal server.


Changes in 0.11
---------------
1. all comments change to /*  */.
2. Added new bit fields in eSCI CR2.
3. Fixed eQADC, edma and eTPU register spacing.
4. typedefs.h updated to support GHS.
5. mpc5500_utils file renamed to etpu_utils and removed from header files zip file.

Changes in 0.10
---------------
1. Fixed some mistake in bit field and registers.
2. Included mpc5500_util.c/h file. The function have not been fully debugged yet
    but can be used to get the eTPU working.

CHANGES in 0.09
---------------
1. Fixed a couple bit field names to match 1.0 user's manual that were missed in 0.08
2. Fixed eDMA TCD structures.

CHANGES in 0.08
---------------
1. New register names to match 1.0 user's manual.
2. FMPLL - The bit field in the SYNCR register have changed. MFD is now 5 bits.
The way the MFD values are used has also changed. Writing to the whole register
will give the same results. If you do a write to the MFD bit field, the value
will need to be left shifted by 1.
3. DSPI - TCR register is now 32 bits, this was a mistake in earlier versions of the
header files. The active bits are in the upper part of the register so a change to
existing code might be needed.
4. ETPU - Register names changes to end in _A/_B rather than _1/_2.